This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS V6.2 Installation method during anti virus program still running

Tool/software: Code Composer Studio

Hello.I'm using CCsv.6

I was CCS v6 and v3 for a past 10years. but last month my company PC changed to new one. So, I want to install again the CCS v6

but not able to install the CCS V6 due to anti virus program.

due to my company policy, im not able to turned of the anti virus program.

Can i install the CCS v6 without turn off the anti virus program?

  • Hi,

    pilgyum kim said:
    Can i install the CCS v6 without turn off the anti virus program?

    You can try to turn off the protection of certain areas of the system - usually the antivirus software prevents the installer from:

    - writing to non-standard areas of the disk, such as C:\ti (the default installation directory). You can try to see if CCS installs in another directory. However, this may not overcome the next issue.

    - installing the necessary device drivers for the Debug Probes into the Windows System directory. For that you have absolutely no way to workaround this problem. The drivers must be installed. 

    In your particular case, if the company prevents you from configuring your Antivirus software to allow writing on these areas, you will have to refer to your IT department and let them install Code Composer Studio for you. 

    Regards,

    Rafael