This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM3358: Bare-metal code

Part Number: AM3358

Tool/software: Code Composer Studio

Dear team,

we are developing application using AM3358 sitara processor.

IDE used for the same are CCS and ECLIPSE.

we want RAW code for all the protocols used for communication like SPI, I2C,UART etc

Also wants to interface FLASH, SD card etc  with processor.

As of now we have starter ware with us, but it would be more helpful if we get the raw code/driver code for the above mentioned details.

It would be appreciable if we get any link or site from TI including these except starter ware, as we already have it.

can we get direct contact  for support and training so that we can be able to co-ordinate with you.

your quick response is highly appreciated.