Part Number: PROCESSOR-SDK-AM335X
Tool/software: Code Composer Studio
Goodmorning,
I'm working with CCS 7.3 installed on Ubuntu 16.04 and I'm using a Beaglebone Black.
I'm trying to crosscompile an application which uses the ethernet port connected to a secondary device; hence I cannot deploy the application through that port.
I have a further connection with an USB-UART converter with which I can connect to Beaglebone console.
Is it possible to transfer the executable and launch it via UART? And if not what other options do I have?
Thank you.
Regards,
Davide Brunelli