I am using CCSv4.1.3.00034 and set up a project in my workspace with no linked files. This project was building with no problems. I then wanted to add a second project into my workspace so I right clicked in the tree view and selected add new ccs project. I changed the default location to point to the source and header folders on my hardrive. I then started to update the build properties on the second project. I updated the include path and this is where my problem started. The first project in my workspace took on the include path of my second project. See attached views - these are from my first project
You can see from the screen shots that my include options path is still showing the intended include paths but when I look at the high level view the command line is blank - as seen in the second screen shot. Any thoughts?
Thanks,
Scott