Part Number: CC1350
Other Parts Discussed in Thread: SIMPLELINK-CC13X0-SDK
Tool/software: Code Composer Studio
This is the customer request, I would be happy if you can help,
"
We are using Texas Instruments CC1350f128 and using Code composer studio. Which based ti_rtos and for communication easylink library.
We have one transmitter and one receiver, the question is ;
During the communication b/w transmitter and receiver I stop to send data after 9min 27 sec when i send data again there is no communication until 10min 33sec later its connecting.
But during (9:27-10:33) there is no communication except that there is a communication. This always happens at same time where connection is lost. I realized that transmitter sends the data but receiver doesn’t receive What might be the reason for this ?
I investigated easylink lib. During the communication the status when received the packet it is easylink_status_success but during when it doesn’t receive it is easylink_status_busy_error.
Is that might be the reason?
The code is has simply two tasks one rx(receiver) and tx(transmitter). When processor awake first waits in receiver mode and when receives packet changes to transmitter mode and sends a packet than again receiver mode, until it doesn’t receive packet it waits in receiver mode.
"
I would like to share the codes from the customer which is NDA information, please email me privately since i can not share with public.
Thanks in advance