Part Number: TMS320F28377D
Tool/software: Code Composer Studio
Hi Guys, I have a serious problem with CCS9.
My assembler code has just reached 38K and the largest FLASH BANK in the F28377D is 32K from a total of 1MB FLASH. When building my code CCS9 errors saying this:
error #10099-D: program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x814c page 0. Available memory ranges:
FLASHB size: 0x2000 unused: 0x1efd max hole: 0x1efb
FLASHC size: 0x2000 unused: 0x2000 max hole: 0x2000
FLASHD size: 0x2000 unused: 0x2000 max hole: 0x2000
FLASHE size: 0x8000 unused: 0x8000 max hole: 0x8000
error #10010: errors encountered during linking; "max1010_gpu.out" not built
How can I tell CCS9 to write my code starting from FLASH A and then continue to FLASH B, then C, then D and so on until the end of flash memory.
My F28377D has 1MB of flash memory, and I can only use 32K of it. I'm not to happy about that.
Please help as this is quite urgent.
Thanks Guys
Pete