This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Merging boot and application hex files

Other Parts Discussed in Thread: MSP430F149

I have two projects.  A custom bootloader and an application project.  They share some common data that will live in the bootloader code.  Also I have created interrupt jump tables in the bootloader much like the CCS_ISR_Sample_Program attached in an earlier posting.

1) Is there a tool available to merg the two into one hex file?  Or are there options in the project Build Steps that can be used to do this?

2) Is there a tool or option that will strip off areas of the hex files?

3) I am sure you cannot debug both projects at once but is there a way you can debug with the source loaded from both programs?

 

Thank you for your help

Tom