After breaking out of our batch file base build process, I received the following information:
INTERNAL ERROR: c:\ti_dsp.tms470\bin\cg470.exe experienced a fatal internal fault while
processing function _RelDump file rldump.c line 3399
This is a serious problem. Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.
I unfortunately cannot provide the source file as an attachment due to confidentiality. Needless to say that the file in question is nearly 128K in size. The command line options passed to this file are:
c:\ti_dsp.tms470\bin\cl470
-c
-g
--endian=little
-D=DCL_CPU_ALIGNSIZE=4
-DDCL_BIG_ENDIAN=0
-pden -pdsr=190
-D=D_PRODUCTNUM=1
-D=D_PRODUCTVER=0x02000000
-D=D_PRODUCTBUILD=1874P
-D=D_TOOLSETNUM=10000
-D=D_CPUFAMILY=D_CPUFAMILY_armv5tej
-D=D_CPUTYPE=arm926ejs
-D=D_DEBUG=1
-D=D_OSVER=n/a
--diag_remark 188
--verbose_diagnostics
-I=c:\ssp_datalight\rtos\reliance\source\projects\rtos\armboot
-I=c:\ssp_datalight\rtos\reliance\source\os\rtos\include
-I=c:\ssp_datalight\rtos\reliance\source\include
-I=c:\ssp_datalight\rtos\reliance\source\dcl\os\rtos\include
-I=c:\ssp_datalight\rtos\reliance\source\dcl\include
-I=c:\ssp_datalight\rtos\reliance\source\core\nitro\include
-I="c:\ti_dsp.tms470\include"
-eo=.obd rldump.c
Please let me know how to contact you to possibly provide more detail, or if you can provide me information about additional command line parameters I could pass to the compiler to get you more information.