Other Parts Discussed in Thread: UCD3138
Tool/software: Code Composer Studio
1.How many watts does UCD3138 consume?
2.To enhance efficiency of very light load(2~5% load), the power loss of UCD3138 is a keypoint. How can I to reduce the power loss of UCD3138?
3.The output voltage of aux. power is 12V and the used voltage of UCD3138 is 3.3V. The voltage should be converted from 12V to 3.3V, the linear converter is easy to used but much loss is needed. Can I use the switching power converter to convert the needed voltage?