I'm currently running CCS4 v4.1.3.00038 with CGT v3.2.1. How do I update just my CGT to v3.3.0 to keep in sync with my software developer who is running CCS4 v4.1.3.00038 and CGT v3.3.0?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mike,
Go to Help->Software Updates->Find and Install
Select "Search for new features to install"
Check the "Code Generation Tools Updates" box
Click Finish
You can expand the tree to show the various compiler updates.
By default it will only show the patch for each version class (i.e. 3.3.2 and not 3.3.0 and 3.3.1). If you uncheck the box to "Show the latest version of a feature only" then it should show the rest of the releases.
Regards,
John
Thanks John,
The only options I have under "Search for new features to install" are:
1. Blackhawk CCSv4 Emulation Updates
2. Code Composer Studio Updates
3. Spectrum Digital CCS4.2 Emulation Updates.
I don't see "Code Generation Tools Updates" as being an option at all. Suggestions? Is my CCS install hosed for some reason?
Is 3.3.1 ok or do you have to have 3.3.0? The reason I ask is that I need to give you a feature file for Eclipse and the one I have is 3.3.0 so if I give you that then you wouldn't see it when checking for updates.
I am going to try sending you a private message with a link to an update site to add.
John