This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352P: I2C and Timer driver initialization error

Part Number: CC1352P
Other Parts Discussed in Thread: SYSCONFIG

Tool/software: Code Composer Studio

Hi All,

We were developed an application based on "simplelink_cc13x2_sdk_2_30_00_45".

Now because of Silicon Revision we are porting our application with newer SDK "simplelink_cc13x2_26x2_sdk_3_30_00_03".

Here it is showing some compilation error on I2C and GPTimer initialization.

Kindly someone suggest idea on this. Attached the image for reference.

Thanks & Regards,

Yasar Arafath