This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: IWR1443 BOOST

Part Number: IWR1443BOOST

Tool/software: Code Composer Studio

Hi,

Trying to debug with mmWave DevPack.

Loading program failed:

Cortex_R4_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x3c: This operation is not supported by this driver
Cortex_R4_0: File Loader: Verification failed: Target failed to write 0x00000000
Cortex_R4_0: GEL: File: C:\Users\spriyanka\Downloads\CCS9.2.0.00013_win64\vitalSigns_lab\Debug\xwr14xx_vitalSigns_lab_mss.xer4f: Load failed.

 

Texas Instrument XDS110 USB Debug probe is not getting loaded

 

Help me to reolve this issue..

  • Priyanka,

    Looking at the screen capture I can see that you have "Data Snapshot Viewer" selected as your debug connection type instead of an XDS110.

    You can change this in the target configuration file (.ccxml).  I am not sure if this is a file that is part of a project or if you created it separately.  I am guessing separately since the debug session is not for a project.  If you open the target configuration file in the editor you can change the connection type:

    Regards,

    John