Part Number: LP-MSP430FR2476
Tool/software: Code Composer Studio
What are the steps to compile the Out of Box Experience for the LP-MSP430FR2476?
SLAU802, page 17, section 4.1.2 indicates I need to be running CCS v8.0 or higher. I'm running 9.2. It says "... click Project>Import Existing CCS Eclipse Project. Browse to desired demo project directory that contains main.c (see Figure 13)." There is no tab under Project to Import Existing CCS Eclipse Project.
I've tried creating my own project, unzipping, the example files, and copying required .h files up to the project directory since the tool can't seem to see them in lower directories even if I adjust the include paths for the compiler invocation command.
I am completely stuck. Any help will be appreciated. Thanks.
Richard