Part Number: MSP432P4111
Tool/software: Code Composer Studio
Hi,
I'm new with RTOS and I'm trying to connect a display to the MSP-EXP432P401R using UART1. In the display there is a keyboard and numbers are sent to the TI board, and then they are sent again to my laptop using UART0:
while(1) {
UART_read(uart1, &input, 1);
UART_write(uart, &input, 1);
}
The parameters are:
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 115200;
But I don't see anything in my terminal. I know that the display is working properly, so I can't understand why the MSP-EXP432P401R doesn't receive the numbers on UART1.
Thanks.
Best regards,
Samuele