This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS 8.2 cause C/C++ Indexer rebuild full index

Tool/software: Code Composer Studio

[The issue]:

In CCS 8.2, when C file is modified and save. The C/C++ Indexer is triggered to rebuild FULL index. It takes tens of minutes to rebuild full index.

[Observation]:

After removed all TI CCS 8.2 components, the Eclipse C/C++ Indexer performs as expected and rebuild only modified file. It takes one second to index modified file.

[Project type]:

C/C++ Make file with existing code.

Based on the observation, it looks like some components in CCS always trigger full index rebuild, which is not expected and make CCS difficult to use.

  • Hi Jerry,

    We had several indexer issues in CCSv8.x. When we fixed some issues in on 8.x version, others got introduced in the next 8.x version. 

    If possible, I would recommend updating to CCSv9.x. If there is some limitation that prevents you from moving to CCSv9 (ex. you are using 32-bit Windows or you are using XDS510 class debug probes), then please try moving to CCSv8.3.1.

    Thanks

    ki


  • Hello,
    I haven’t heard back from you, hence this issue is being closed. If you wish to continue the discussion, please post a reply with an update below (or create a new thread).

    Thanks,
    ki