This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1843BOOST: #1965 can not open source file issue

Part Number: AWR1843BOOST

Tool/software: Code Composer Studio

Hi,

I use the CCS v8.3 to build the sample code.

When I restart the PC, my CCS IDE build the mss project happens the #1965 can not open source file issue. 

As below:

I make sure that the mmw_config.h file has exist in "ti/demo/io_interface" path.

Is there a good solution for this issue?

Thank you.

  • HI,

    Could you check CCS project properties->Resource->Linked Resources and check 'COM_TI_MMWAVE_SDK_INSTALL_DIR' MACRO value. It should link to the existing SDK path.

    At the same SDK path you need to copy mmw_cnonfig.h

    Regards,

    Jitendra