This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem for running MSP-EXP430G2-LaunchPad demo

Other Parts Discussed in Thread: MSP430G2001

I have got a MSP-EXP430G2-LaunchPad demo. and following the instruction of "Getting Started with the MSP430 LunchPad" to step 10. every thing looks cool to me. However, when I went to step 11, that I clicked "Build" button and watch the tools run in Console window. There are a lot error messages (in Red) as follows, I prety sure that I have not done anything wrong and changed any C program codes. I just pasted the Code from .txt to main.c and save it. Why have I had the following error messages, and how to fix them? Thanks 

 

"../lnk_msp430g2001.cmd", line 60: error: placement fails for object ".text",

size 0x5b2 (page 0). Available ranges:

FLASH size: 0x1e0 unused: 0x1c0 max hole: 0x1c0

 

undefined first referenced

symbol in file

--------- ----------------

ADC10CTL0 ./main.obj

ADC10CTL1 ./main.obj

ADC10MEM ./main.obj

 

error: unresolved symbols remain

error: errors encountered during linking; "Temperature_Sense_Demo.out" not

built

 

>> Compilation failure

gmake: *** [Temperature_Sense_Demo.out] Error 1

gmake: Target `all' not remade because of errors.

Build complete for project Temperature_Sense_Demo.