Other Parts Discussed in Thread: MSPMATHLIB
Tool/software: Code Composer Studio
Hello,
I try to compile the RELEASE version of my project but the CCS reports the following error:
undefined first referenced
symbol in file
--------- ----------------
__TI_int53
__TI_int61
error #10234-D: unresolved symbols remain
warning #10202-D: no suitable entry-point found; setting to 0
error #10010: errors encountered during linking; "MCURF430F5155.out" not built
gmake[1]: *** [MCURF430F5155.out] Error 1
gmake[1]: Target 'secondary-outputs' not remade because of errors.
gmake: *** [all] Error 2
makefile:167: recipe for target 'all' failed
The strange thing is the DEBUG version is compiled (and outputs the *.out file).
Attached:
the RF430F5155.h file used on the project.
Below you find:
1. the report of the compilation in RELASE version (which report error)
2. the report of the compilation in DEBUG version (which is OK)
Thank you in advance for your help!
Best regards.
Alessandro
**** Build of configuration Release for project MCURF430F5155 ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O
Building target: "MCURF430F5155.out"
Invoking: MSP430 Linker
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --code_model=small -O2 --use_hw_mpy=F5 --advice:power=all --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal -z -m"MCURF430F5155.map" --stack_size=80 --heap_size=80 -i"C:/ti/ccsv8/ccs_base/msp430/include" -i"C:/ti/ccsv8/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/ti/ccsv8/tools/compiler/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --absolute_exe --xml_link_info="MCURF430F5155_linkInfo.xml" --use_hw_mpy=F5 --rom_model -o "MCURF430F5155.out" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_CA/Out/cmd.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_CA/Out/pke.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_EEPROM/Out/eeprom.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF/Out/lf.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF/Out/lf_dll.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_PROG_FRAME/Out/main.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_PROG_FRAME/Out/vector.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out/rf.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out/rf_dll.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out/rf_phy.obj" "../lnk_rf430f5155.cmd" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_FRANTIC/Out/frantic.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF_FRONT/Out/craidaes.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LOCAL_IO/Out/local_io.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_MATH/Out/crc.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RKE/Out/rke.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_SPI/Out/spi.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_TIMING/Out/timing_rf430f51xx.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_BATTERY/Out/battery.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_TIMING/Out/timing.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_DEBUG/Out/debug.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_DIAGNOSIS/Out/diagnosis.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_DIAGNOSIS/Out/diagnosis_eol.obj"
<Linking>
warning #10208-D: automatic RTS selection: attempt to automatically link in index library "libc.a" failed; file not found
remark #10372-D: (ULP 4.1) Detected uninitialized Port A in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
"../lnk_rf430f5155.cmd", line 222: warning #10374-D: Interrupt vector "ADC10" does not have an interrupt handler routine.
remark #10372-D: (ULP 4.1) Detected uninitialized Port B in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
remark #10422-D: (ULP 6.2) Detected use of a device with available 32-bit hardware multiplier and not also using MSPMATHLIB library (libmath.a). Recommend using MSPMATHLIB library (libmath.a) for improved performance.
>> Compilation failure
makefile:171: recipe for target 'MCURF430F5155.out' failed
"../lnk_rf430f5155.cmd", line 230: warning #10374-D: Interrupt vector "UNMI" does not have an interrupt handler routine.
warning #10062-D: entry-point symbol "_c_int00" undefined
undefined first referenced
symbol in file
--------- ----------------
__TI_int53
__TI_int61
error #10234-D: unresolved symbols remain
warning #10202-D: no suitable entry-point found; setting to 0
error #10010: errors encountered during linking; "MCURF430F5155.out" not built
gmake[1]: *** [MCURF430F5155.out] Error 1
gmake[1]: Target 'secondary-outputs' not remade because of errors.
gmake: *** [all] Error 2
makefile:167: recipe for target 'all' failed
**** Build Finished ****
**** Build of configuration Debug for project MCURF430F5155 ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O
Building file: "../MOD_CA/Source/cmd.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power="all" -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_CA/Out" --preproc_with_compile --preproc_dependency="MOD_CA/Source/cmd.d_raw" "../MOD_CA/Source/cmd.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
Finished building: "../MOD_CA/Source/cmd.c"
Building file: "../MOD_CA/Source/pke.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power="all" -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_CA/Out" --preproc_with_compile --preproc_dependency="MOD_CA/Source/pke.d_raw" "../MOD_CA/Source/pke.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_CA/Source/pke.c", line 94: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_CA/Source/pke.c", line 96: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
"../MOD_CA/Source/pke.c", line 96: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
"../MOD_CA/Source/pke.c", line 97: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
"../MOD_CA/Source/pke.c", line 127: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_CA/Source/pke.c", line 129: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
"../MOD_CA/Source/pke.c", line 129: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
"../MOD_CA/Source/pke.c", line 203: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_CA/Source/pke.c", line 205: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
"../MOD_CA/Source/pke.c", line 205: remark #2553-D: (ULP 14.1) Array index (involving "U8_loop_counter") of type "int". Recommend using "unsigned int"
Finished building: "../MOD_CA/Source/pke.c"
Building file: "../MOD_EEPROM/Source/eeprom.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_EEPROM/Out" --preproc_with_compile --preproc_dependency="MOD_EEPROM/Source/eeprom.d_raw" "../MOD_EEPROM/Source/eeprom.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_EEPROM/Source/eeprom.c", line 120: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_EEPROM/Source/eeprom.c", line 127: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_EEPROM/Source/eeprom.c", line 163: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_EEPROM/Source/eeprom.c", line 170: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_EEPROM/Source/eeprom.c", line 185: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_EEPROM/Source/eeprom.c", line 192: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
Finished building: "../MOD_EEPROM/Source/eeprom.c"
Building file: "../MOD_LF/Source/lf.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF/Out" --preproc_with_compile --preproc_dependency="MOD_LF/Source/lf.d_raw" "../MOD_LF/Source/lf.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_LF/Source/lf.c", line 84: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
Finished building: "../MOD_LF/Source/lf.c"
Building file: "../MOD_LF/Source/lf_dll.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF/Out" --preproc_with_compile --preproc_dependency="MOD_LF/Source/lf_dll.d_raw" "../MOD_LF/Source/lf_dll.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_LF/Source/lf_dll.c", line 22: remark #2553-D: (ULP 14.1) Array index (involving "U8_length") of type "int". Recommend using "unsigned int"
Finished building: "../MOD_LF/Source/lf_dll.c"
Building file: "../MOD_PROG_FRAME/Source/main.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_PROG_FRAME/Out" --preproc_with_compile --preproc_dependency="MOD_PROG_FRAME/Source/main.d_raw" "../MOD_PROG_FRAME/Source/main.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_PROG_FRAME/Source/main.c", line 769: warning #177-D: subscript out of range
"../MOD_PROG_FRAME/Source/main.c", line 802: warning #177-D: subscript out of range
"../MOD_PROG_FRAME/Source/main.c", line 912: warning #177-D: subscript out of range
"../MOD_PROG_FRAME/Source/main.c", line 385: warning #179-D: variable "U8_fg_tx_todo" was declared but never referenced
"../MOD_PROG_FRAME/Source/main.c", line 386: warning #179-D: variable "U8_serial_number_dbg" was declared but never referenced
"../MOD_PROG_FRAME/Source/main.c", line 387: warning #179-D: variable "U8_Eeprom_Data_dbg" was declared but never referenced
"../MOD_PROG_FRAME/Source/main.c", line 388: warning #179-D: variable "U8_lf_data_dbg" was declared but never referenced
Finished building: "../MOD_PROG_FRAME/Source/main.c"
Building file: "../MOD_PROG_FRAME/Source/vector.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_PROG_FRAME/Out" --preproc_with_compile --preproc_dependency="MOD_PROG_FRAME/Source/vector.d_raw" "../MOD_PROG_FRAME/Source/vector.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
Finished building: "../MOD_PROG_FRAME/Source/vector.c"
Building file: "../MOD_RF/Source/rf.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out" --preproc_with_compile --preproc_dependency="MOD_RF/Source/rf.d_raw" "../MOD_RF/Source/rf.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_RF/Source/rf.c", line 65: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_RF/Source/rf.c", line 145: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../MOD_RF/Source/rf.c", line 201: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../MOD_RF/Source/rf.c", line 253: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../MOD_RF/Source/rf.c", line 258: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../MOD_RF/Source/rf.c", line 332: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../MOD_RF/Source/rf.c", line 337: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../MOD_RF/Source/rf.c", line 367: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
Finished building: "../MOD_RF/Source/rf.c"
Building file: "../MOD_RF/Source/rf_dll.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out" --preproc_with_compile --preproc_dependency="MOD_RF/Source/rf_dll.d_raw" "../MOD_RF/Source/rf_dll.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_RF/Source/rf_dll.c", line 34: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_RF/Source/rf_dll.c", line 36: remark #2553-D: (ULP 14.1) Array index (involving "i") of type "int". Recommend using "unsigned int"
"../MOD_RF/Source/rf_dll.c", line 51: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_RF/Source/rf_dll.c", line 53: remark #2553-D: (ULP 14.1) Array index (involving "i") of type "int". Recommend using "unsigned int"
Finished building: "../MOD_RF/Source/rf_dll.c"
Building file: "../MOD_RF/Source/rf_phy.c"
Invoking: MSP430 Compiler
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --include_path="C:/ti/ccsv8/ccs_base/msp430/include" --include_path="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155" --include_path="C:/ti/ccsv8/tools/compiler/include" --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal --obj_directory="C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out" --preproc_with_compile --preproc_dependency="MOD_RF/Source/rf_phy.d_raw" "../MOD_RF/Source/rf_phy.c"
>> WARNING: --near_data is only applicable for large data models. Option ignored.
"../MOD_RF/Source/rf_phy.c", line 26: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
"../MOD_RF/Source/rf_phy.c", line 28: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
"../MOD_RF/Source/rf_phy.c", line 28: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
Finished building: "../MOD_RF/Source/rf_phy.c"
Building target: "MCURF430F5155.out"
Invoking: MSP430 Linker
"C:/ti/ccsv8/tools/compiler/bin/cl430" -vmsp --abi=coffabi --near_data=globals --use_hw_mpy=F5 --advice:power=all -g --define=__RF430F5155__ --display_error_number --diag_warning=225 --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --printf_support=minimal -z -m"MCURF430F5155.map" --stack_size=80 --heap_size=80 -i"C:/ti/ccsv8/ccs_base/msp430/include" -i"C:/ti/ccsv8/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/ti/ccsv8/tools/compiler/lib" -i"C:/ti/ccsv8/tools/compiler/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="MCURF430F5155_linkInfo.xml" --use_hw_mpy=F5 --rom_model -o "MCURF430F5155.out" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_CA/Out/cmd.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_CA/Out/pke.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_EEPROM/Out/eeprom.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF/Out/lf.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF/Out/lf_dll.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_PROG_FRAME/Out/main.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_PROG_FRAME/Out/vector.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out/rf.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out/rf_dll.obj" "C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RF/Out/rf_phy.obj" "../lnk_rf430f5155.cmd" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_FRANTIC/Out/frantic.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LF_FRONT/Out/craidaes.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_LOCAL_IO/Out/local_io.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_MATH/Out/crc.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_RKE/Out/rke.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_SPI/Out/spi.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_TIMING/Out/timing.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_TIMING/Out/timing_rf430f51xx.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_BATTERY/Out/battery.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_DEBUG/Out/debug.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_DIAGNOSIS/Out/diagnosis.obj" -l"C:/Users/alessandroserafini/workspace_v8/MCURF430F5155/MOD_DIAGNOSIS/Out/diagnosis_eol.obj" -llibc.a -llibmath.a
<Linking>
>> WARNING: --near_data is only applicable for large data models. Option ignored.
warning #10204-D: could not resolve index library "libmath.a" to a compatible library
remark #10372-D: (ULP 4.1) Detected uninitialized Port A in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
remark #10372-D: (ULP 4.1) Detected uninitialized Port B in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
Finished building target: "MCURF430F5155.out"
Building files: "MCURF430F5155.out"
Invoking: MSP430 Hex Utility
"C:/ti/ccsv8/tools/compiler/bin/hex430" --memwidth=8 --romwidth=8 --intel -o "MCURF430F5155.hex" "MCURF430F5155.out"
Translating to Intel format...
"MCURF430F5155.out" .text ==> .text
"MCURF430F5155.out" .const ==> .const
"MCURF430F5155.out" .cinit ==> .cinit
"MCURF430F5155.out" PORT2 ==> PORT2
"MCURF430F5155.out" PORT1 ==> PORT1
"MCURF430F5155.out" TIMER1_D1 ==> TIMER1_D1
"MCURF430F5155.out" TIMER1_D0 ==> TIMER1_D0
"MCURF430F5155.out" TEC1 ==> TEC1
"MCURF430F5155.out" DMA ==> DMA
"MCURF430F5155.out" TIMER0_A1 ==> TIMER0_A1
"MCURF430F5155.out" TIMER0_A0 ==> TIMER0_A0
"MCURF430F5155.out" ADC10 ==> ADC10
"MCURF430F5155.out" USCI_B0 ==> USCI_B0
"MCURF430F5155.out" USCI_A0 ==> USCI_A0
"MCURF430F5155.out" WDT ==> WDT
"MCURF430F5155.out" TIMER0_D1 ==> TIMER0_D1
"MCURF430F5155.out" TIMER0_D0 ==> TIMER0_D0
"MCURF430F5155.out" TEC0 ==> TEC0
"MCURF430F5155.out" COMP_B ==> COMP_B
"MCURF430F5155.out" UNMI ==> UNMI
"MCURF430F5155.out" SYSNMI ==> SYSNMI
"MCURF430F5155.out" .reset ==> .reset
Finished building: "MCURF430F5155.out"
**** Build Finished ****