Part Number: TIDA-01485
Tool/software: Code Composer Studio
HI there,
I tried to evaluate TIDA-01485 with MSP FET flash emulation tool. following the instruction, downloading the CCS9.2 ( only installed MSP430 related) and the example firmware TIDA-01485_Firmware_V1.0, there are a bunch of compilation and linking errors, such as cannot find stdin.h etc.
after delete and reinstall the firmware, then some undefined symbol appear, which I cannot search for within the workspace
undefined first referenced
symbol in file
--------- ----------------
_delay_cycles ./main.obj
_disable_interrupt ./main.obj
error #10234-D: unresolved symbols remain
I am not sure if I installed the CCS9.2 correctly or I also have to configure the project instead of simply import to CCS? Do you have any document for the TIDA-01485 project compiling, progarmming, and tsting thanks!