Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: CC2640
Tool/software: Code Composer Studio
Hello,
I have been using the cc2640 launchpad for some time, but yesterday when I tried to burn load program to the launchpad, it showed a warning for a firmware update. when I selected update now, it failed to get updated and following it, it ran into an error listed below
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Warning: A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect it to the debug target. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 8.3.0.00003)
Cortex_M3_0: Error: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 8.3.0.00003)
Cortex_M3_0: GEL: Error while executing StartUp( 9, 2, 0, 1751 ): Reset failed: retcode=-1
at GEL_AdvancedReset("Board Reset") [cc26x0.gel:29]
at StartUp(9, 2, 0, 1751)
IcePick_C: Error connecting to the target: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 8.3.0.00003)
when I tried using smart rf flash programmer 2, it shows for update every time I open it and when I select update now, it shows an update is completed but when I reopen it after some time it again asks for an update.
Also, smart rf flash programmer 2 is not recognizing the launchpad.
Please check attached screenshots