This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMDSDSK6455: compile and debug code out side of code composer studio

Part Number: TMDSDSK6455


Tool/software: TI C/C++ Compiler

Hi all,

can I compile and debug code outside of the code composer studio?

for example on visual studio,clion, etc..

if I can, please explain a bit

Thanks,

Saeed

  • It is possible to build outside of CCS, with a makefile or something similar.  Then you can use CCS to debug the resulting executable.  

    If you want to debug with a tool other than CCS ... There are probably some debuggers for the 6455 DSK other than CCS.  But I don't know anything about them.  If you really want to explore that, then I need to get some other experts to help.

    Thanks and regards,

    -George