This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS 's graph y axis value issue



Tool/software: Code Composer Studio

Hi:

I want use graph to show a variable .    but I don't konw the Y axis value means   .  can you  tell me ?     definitely,  that  is no IQ 24 .   because   clarck.As  just is < IQ(0.2) .    

best regard !

  • Hello,

    Yes, something does not look right. Can you try resetting the graph and then refreshing it?

    Thanks

    ki

  • Hello,

    Just checking to see if you had a chance to try resetting the graph and then refreshing it.

    Thanks

    ki

  • hi, ki  thank you

    I try every thing you said . but  have not  resolved .     I even think  "graph" i not use in ccs6.2     ,,   I use ccs from 3.3 to 6.2 .    find   3.3 graph is ok  ,,    but from ccs4 to ccs8 .   I can not hold it . 

    From ti program show :

    but for me , same program ,   when i use graph ,  the graph show some thing I don't kow what it is .   I look <<help >>, say that set easy .   

    so please help ,  that is big issue for me !

    best regard . 

  • yanzhen fu said:
    I use ccs from 3.3 to 6.2 .    find   3.3 graph is ok  ,,    but from ccs4 to ccs8 .   I can not hold it . 

    That is odd. CCS versions later the 3.3 also support dual time graphs. Actually, the implementation of the graph feature should be the same as it was in v3.3.

    Can you show me a screenshot of what you see in CCSv6.x?