This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v4 Image Analizer

Hello,

In CCS v4 there is a feature "Image Analyzer" which is supposed to read for example .yuv file loaded in memory and display it as visible image. What I am trying to do is convert a graphic into .yuv. Then load it in memory using the CCS feature, then read this graphic into the ISS OMAP4430 hardware, do some image manipulations and write it back to memory. Then using again the image analyzer see the changes made by the ISS.

Right now I am stuck on displaying the image simply from memory into the window of the analyzer. I tried converting various images (jpeg, etc) into .yuv loading them to memory and scan them with the analyzer. Does anyone know a convertor, or even better a help source how to work with the CCS v4 image analyzer?

Any help is appreciated

Thanks a lot,

Best regards,

Alex