Tried to do port connect with CCS4 and C6678 simulator
Got the following error message:
TMS320C66x_0: Error during port connect: Port connect not supported on this simulator configuration I use CCS4 with version 4.1.0.02006 and teh simulator is tisim66xxx_joule_multi.dvr version 10.1.117.0 1. Is this a known issue or I do something wrong? 2. If this is a problem, was it corrected in other versions of teh simulator? Thanks Ran