Hi,
I wonder if the CCS3.3 code gen tool for C2000 is still being updated and what might be the latest version? Comparing the code generated from CCS4.2 or CCS3.3, if I use the same code generation tool version, am I getting the same image .out file? If not, what else do I need to update in the 3.3 to keep the code generated identical to that from a latest CCS4?
Thanks
Leong