This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F280049C: GEL Error: identifier ST1 not found /// identifier not found: XAR0

Part Number: LAUNCHXL-F280049C


Tool/software: Code Composer Studio

Hello, 

When I tried to load my program in the board on my computer, it worked fine, however I need to be able to debug the code in another computer. When I tried loading the code I got  this error:

C28xx_CPU1: GEL: Error while executing OnTargetConnect(): identifier not found: ST1
  at ST1=(ST1&~(0x0100)) [f280049m.gel:286]
  at C28x_Mode() [f280049m.gel:92]
  at OnTargetConnect()
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL: Error while executing OnReset(0): identifier not found: XAR0
  at XAR0=*((unsigned long *) 0x78000) [f280049m.gel:353]
  at SetupDCSM() [f280049m.gel:33]
  at OnReset(0)
C28xx_CPU1: File Loader: Verification failed: Values at address 0x00000@Program do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\Users\ANDAR\workspace_v9_2\buffdac_ex1_enable\CPU1_RAM\buffdac_ex1_enable.out: a data verification error occurred, file load failed.

When I test the connection on target configuration page it passes all tests. I tried loading an example code to see if it works and I got the same error. I downloaded the latest version of CCS (9.2.0) and I still get the same error.