Hi folks,
This is the first time I am using CCS 4 and DSP F28335.
I am Using CCS4 (30 day trial version) with DSP F28335's experimental docking Board (TMDSDOCK28335) which I believe has the on board XDS100 emulator. And this is the connection that I am using to make the PC- DSP connection.
I followed the cook book approach to run my first project, i.e. the CPU_timer project using the wiki on C2000 Getting started with CCS V4 and document SPRCA73.
After much toil, I was able to run it successfully as I could see the "Cputimer"s increment every second in the "Watch" window.
I tried to follow the same approach to rerun the sample project (CPU_timer) but turns out that it wont work; The Code builds up fine and the timers exhibit the right memory addresses in the "watch" window but they just would not increment with time; their value remains unchanged with time
I even checked the forums and found an earlier post titled "CCS v4 "XDS100 Limited Free License", not supporting real time debug" which addressed problems with a CCSv4 bug having problems with real time monitoring; but turns out my version of CCS 4 has the required files.
Can some one please point as to what could be the reason behind this event? Any help or suggestions will be very highly appreciated.