Part Number: TMS320F28388D
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
I am using two XDS110 emulators connected to CCSv9.2.0.00013 with latest emulation updates.I have two different workspaces and the target configuration differentiates the emulators based on Serial number of the Emulator.
While using the emulators to debug the software on target boards(F28388D based internal development boards). I get this error:
IcePick_C_0: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 8.4.0.00006)
CS_DAP_0: Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.4.0.00006)
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.4.0.00006)
Cortex_M4_0: JTAG Communication Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 8.4.0.00006)
Cortex_M4_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
This error is displayed on both CCS instances. Only a PC reboot helps to recover from this state.
If attempting to connect without a Reboot CCS displays an Error message:
Error connecting to the target:
(Error -261 @ 0x0)
Invalid response was received from the XDS110.
(Emulation package 8.4.0.00006)
Regards,
Sudharsanan