Hi,
I've just received C6A816x evaluation module and I wanted to test it with TI "big time" example but when I try to connect to EVM I get this error message
Error connecting to the target:
Error 0x80000244/-1265
Fatal Error during: Register, Initialization, OCS,
The TAP ID for the DAP, read as 0x00000000, does not match with the default ID or the one provided in the board file.
OS windows 7 64bits
CCS Version: 4.2.1.00004
C6A816x/AM386x evaluation module
Emulator XDS100V2
There isn't any TI816x platform to select while doing target configuration.
I also tried with XDS510 but I don't have any connection at all with the EVM .
Any help would be great.