Part Number: CC1352P
Tool/software: Code Composer Studio
I'm using a custom board with the cc1352p. I started using regular JTAG, but switched over to cJTAG as recommended by TI. If I start a debug session and wait a about ~10 seconds or so I start getting the following error:
IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 8.4.0.00006)
I dropped the cJTAG freq to 1MHz thinking it may help.
I'm using Ubuntu18, CCS v9.3 example code for the launchpad cc1352P2