Part Number: TMS320F28027
Tool/software: Code Composer Studio
I m having a TMS320F28027 device, on my PCB, whose schematics is derived from TIDA01292.
when i m doing the test it is giving the following error:
----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.
The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.
[End]
But after the run is completed it is giving the following error:
Error connecting to the target:
(Error -1041 @ 0xFFFFFF49)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 8.0.27.9)
Please help me out in the regard, i replaced the cable, checked clock, dont know where the issue lies