Part Number: CC2650MODA
Tool/software: Code Composer Studio
I'm trying to get my Launchpad with the BLE-MODA board up and running with FreeRTOS (the rest of the crew hasn't used TI-RTOS before)... but I'm not getting very far:
I tried to import the file from C:\ti\simplelink_sdk_ble_plugin_3_20_00_24\examples\rtos\MSP_EXP432P401R\bluetooth\simple_application_processor, but it had an error during the import... but it still put it into the Project Explorer.
I downloaded FreeRTOS and put it into C:\ti\FreeRTOS, and set the environment variable under preferences.
It still wouldn't compile... it was complaining that a lot of files were missing.
I manually copied the c:\ti\FreeRTOS files over to the project... but there seems to be a lot of mismatches/different bits... and when I compile, it complains:
Building file: "../posix/freertos/package/build.cfg"
Invoking: XDCtools
"C:/ti/ccs920/xdctools_3_60_01_27_core/xs" --xdcpath="C:/ti/simplelink_msp432p4_sdk_3_30_00_13/source;C:/ti/simplelink_msp432p4_sdk_3_30_00_13/kernel/tirtos/packages;C:/ti/simplelink_sdk_ble_plugin_3_20_00_24/source;C:/ti/tirtos_msp43x_2_20_00_06/packages;C:/ti/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages;C:/ti/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages;C:/ti/tirtos_msp43x_2_20_00_06/products/uia_2_00_06_52/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M4F -r debug -c "C:/ti/ccs920/ccs/tools/compiler/ti-cgt-arm_18.12.4.LTS" "../posix/freertos/package/build.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring build.xem4f from package/cfg/build_pem4f.cfg ...
posix/freertos/package/subdir_rules.mk:12: recipe for target 'build-1043301905-inproc' failed
js: "./package/cfg/build_pem4f.cfg", line 145: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'ti.platforms.tiva' along the path: 'C:/ti/simplelink_msp432p4_sdk_3_30_00_13/source;C:/ti/simplelink_msp432p4_sdk_3_30_00_13/kernel/tirtos/packages;C:/ti/simplelink_sdk_ble_plugin_3_20_00_24/source;C:/ti/tirtos_msp43x_2_20_00_06/packages;C:/ti/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages;C:/ti/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages;C:/ti/tirtos_msp43x_2_20_00_06/products/uia_2_00_06_52/packages;C:/ti/ccs920/xdctools_3_60_01_27_core/packages;..;'. Ensure that the package path is set correctly.
What version of FreeRTOS should I be using and how do I properly install it into CCS?
Is the ti.platforms.tiva package a separate thing that I need to download and install (and how)?