Hello,
I am working on a project, i am using code composer studio v3.3.
Here i am getting a problem when F2812 board is connected to the ccs3.3.
when i power on the board is connecting with out any problem for 15sec, it is showing halted in ccs, but after 15sec it is disconnecting itself and gets an error.
Here is the following the error that i am getting in ccs,
//Power Failure on Target CPU: Error 0xA0001020/-1062 Error during: Execution, Target, Device driver: Power Loss Detected on Target CPU. This could also result from disconnecting the emulator from the target. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Sequence ID: 16 Error Code: -1062 Error Class: 0xA0001020
can anyone help me out.