Part Number: LAUNCHXL-F28069M
Tool/software: Code Composer Studio
hello,
Once debugging lab2a , an error came up saying this:
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 8.4.0.00006)
Note that I previously debugged the same lab without any debugging errors.
By repeating the debug new errors come up :
Error connecting to the target:
(Error -1135 @ 0x0)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 8.4.0.00006)
I tried to change the cable, with a new one, same error remained.
Could it be power supply error? I am using 9 V battery to spin a small motor.
Can you screenshot how to Unlock the device as recommended above in the error details.
Here is a screenshot of my screen
Thanks ,
Jinan