Part Number: LAUNCHXL-F28027F
Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Tool/software: Code Composer Studio
I'm still fairly unfamiliar with the CCS. A couple weeks ago I was able to push programs to the Launch Pad. I decided up upgrade from 9.2 to 9.3. Now I'm getting a whole slew of errors all over the place. Either the Micro fried itself by being plugged in for the last couple weeks, or the backwards compatibility is very sad.
My computer recognizes the built in debug probe in the device manager. It didn't seem like I had any big issues pointing CCS to the debug probe. I now try to load the Flash version of the "Example_F2802xLEDBlink" program. I already removed the legacy, error causing items, "XDAIS" and "--cdebug_asm_data" that all of the examples seem to contain from legacy stuff.
The build info I'm receiving on the console is the following...
**** Build of configuration Flash for project Example_F2802xLEDBlink ****
"C:\\ti\\ccs930\\ccs\\utils\\bin\\gmake" -k all
Building target: "Example_F2802xLEDBlink.out"
Invoking: C2000 Linker
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c2000_18.12.4.LTS/bin/cl2000" -v28 -ml -mt --define=_DEBUG --define=_FLASH --define=LARGE_MODEL -g --diag_suppress=10063 --diag_warning=225 --verbose_diagnostics --quiet --abi=coffabi --output_all_syms -z -m"Example_F2802xLEDBlink.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c2000_18.12.4.LTS/lib" -i"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c2000_18.12.4.LTS/include" -i"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_examples_drivers/timed_led_blink" -i"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/lib" -i"C:/ti/controlSUITE/libs/math/IQmath/v15c/lib" --reread_libs --issue_remarks --verbose_diagnostics --xml_link_info="Example_F2802xLEDBlink_linkInfo.xml" --entry_point=code_start --rom_model -o "Example_F2802xLEDBlink.out" "./Example_2802xLEDBlink.obj" "../28027_RAM_lnk.cmd" "C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_headers/cmd/F2802x_Headers_nonBIOS.cmd" "C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/lib/driverlib.lib" -l"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd" -lrts2800_ml.lib -lIQmath.lib -llibc.a
remark: automatic RTS selection: linking in "rts2800_ml.lib" in place of index
library "libc.a"
>> Compilation failure
makefile:145: recipe for target 'Example_F2802xLEDBlink.out' failed
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 71: error:
RAMM0 memory range has already been specified
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 71: error:
RAMM0 memory range overlaps existing memory range RAMM0
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 75: error:
BEGIN memory range has already been specified
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 81: error:
IQTABLES memory range has already been specified
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 81: error:
IQTABLES memory range overlaps existing memory range IQTABLES
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 82: error:
IQTABLES2 memory range has already been specified
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 82: error:
IQTABLES2 memory range overlaps existing memory range IQTABLES2
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 83: error:
IQTABLES3 memory range has already been specified
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 83: error:
IQTABLES3 memory range overlaps existing memory range IQTABLES3
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 85: error:
ROM memory range overlaps existing memory range BOOTROM
ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 86: error:
RESET memory range has already been specified
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 86: error:
RESET memory range overlaps existing memory range RESET
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 93: error:
BOOT_RSVD memory range has already been specified
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 93: error:
BOOT_RSVD memory range overlaps existing memory range BOOT_RSVD
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 94: error:
RAMM1 memory range has already been specified
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
"C:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/cmd/F2802x_generic_flash.cmd", line 94: error:
RAMM1 memory range overlaps existing memory range RAMM1
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
error: errors encountered during linking; "Example_F2802xLEDBlink.out" not
built
gmake: *** [Example_F2802xLEDBlink.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****