This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM5728: AM5728 CCS

Part Number: AM5728

Tool/software: Code Composer Studio

Hi,

I have created a target configuration file for my JTAG connection in CCS9 as follows:-

Connection value is "Texas Instruments XDS2xx USB Debug Probe"

Board or Device value is "GPEVM_AM572X_SiRevA"

Then I click on Save button.

I am getting the following error when I click on "Test Connection" .

[Start: Texas Instruments XDS2xx USB Debug Probe_0]


Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]

-----[Print the board config pathname(s)]------------------------------------

/home/sahil/.ti/ccs930/0/0/BrdDat/testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Texas Instruments XDS2xx USB Debug Probe_0]