Part Number: LAUNCHXL-F28027F
Tool/software: Code Composer Studio
Apologies for the daft question. As i know the tool should do it because ive succeeded in the past.
Ive got a project that is compiled for a different micro, ive changed the configuration file and in the properties, the code will compile and run but it is still targeting the wrong dependency files (the old ones). When ive done this in the past, CCS has created a repo containing all the relevant dependancy files for the micro and its compiled for that micro successfully.
Im running CCS Version: 9.2.0.00013, with the C2000 Compiler. Ive checked for the tool to manage the target config automatically.
Any ideas what im missing? :(
Thanks in advance for your help.