Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
Today I've upgraded to CCS 9.3(os X).
After this I've tried to program my device with XDS110, I was prompt a firmware upgrade and I accepted.
Unfortunately, XDS110 stopped working with error:
CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 8.4.0.00006)
I've tried also with MSPFET and is the same, the only difference is the error: Interface error..
What can I do? When I plug XDS110 the device is not detected anymore.. updating the firmware in the console is also not possible :/
Tried also on windows..
How can I solve this problem?
Thank you for your help