We recently upgraded to CCSv4. Earlier versions used Codewrite or whatever editor the user wished. The base C++ editor that comes with CCSv4 has a limited ability to alter the look of the code. For example, I would like function names in bold so that they stand out from variable names. I don't think this is possible because the syntax preferences for function names are lumped in the same broad category ("Others") as variable names. I can't imagine the majority of CCSv4 users are satisfied with the base editor. Is there a way to define a new editor or a plugin to extend the base editor syntax?