Hi,
I have several problems with CCS (v. 4.1.1.00014) and the emulator.
First I tried to work with it on a Win 7 notebook but I couldn't get CCS recognize the emulator. The hints in this forum ("copy msp430.dll") did not work out.
Then I wanted to uninstall CCS. This didn't work either. And again there was nothing in the forum that could help me ("delete folder manually ... " lol.)
Now I have CCS on Win XP OS. This was okay for a while, however now (maybe one or two weeks later) I have the same error again and I really can't guess what's the problem. The MSP is okay and I don't think that the emulator is damaged because it is still listed in the device manager and windows makes a sound when the emulator is plugged in or out.
Reinstalling CCS didn't improve it, too.
Do you have an suggestions?
Thanks!
Markus
EDIT: I found out that the problem is related to a Microsoft Sidewinder connected via USB. I think there might be a address collision in some way, but I'm not sure. Anyway, the emulator works as long as the Sidewinder isn't connected.