This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3505 Runtime Support Library for CCSv4

Other Parts Discussed in Thread: AM3505

Which should I use?  I'm not using an RTOS.  There are several tiarm7.lib files... are any of these appropriate?  Or is CCSv4 the wrong tool to be used for writing code to run w/o an OS?

  • The AM3505 contains a ARM Cortex A8, so you would need a runtime library built for A8. The ARM code generation tools in CCS4 includes the library rtsv7A8_A_le_n_eabi.lib. This is built for Cortex A8, ARM mode, little-endian, neon support and EABI. If you need a library with support other than these defaults, you can rebuild the runtime library. Please take a look at Chapter 7 of the ARM Compiler Users Guide for details.