Part Number: TM4C1294NCPDT
Tool/software: TI C/C++ Compiler
Hi
I like to combine my bootloader and my application to one file that I could write to the flash of my TM4C1294NCPDT
I tried the
Example 2: User control of load image section formation
from here
https://processors.wiki.ti.com/index.php/Combining_executable_files
I wrote to the rom.cmd file:
--------------------------------------
Bootloader.out
APP.out
--load_image
–o ROM.obj
ROMS
{
Bootloader: origin=0x00000040 len=0x00013cda
APP: origin=0x00019040 len=0x0002adc2
}
-------------------------------------------------------------------
C:\ti\ccs930\ccs\tools\compiler\ti-cgt-arm_18.12.4.LTS\bin\armhex rom.cmd
but with this I get this error:
error: illegal input character: 0xFFFFFFE2
error: illegal input character: 0xFFFFFF80
error: illegal input character: 0xFFFFFF93
fatal error: cannot open input file "o.out": No such file or directory
Did I understand this axample in a wrong way or where is my failure?
Thanks for help
Rene