This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error" expected a declaration"



Hello,

i use CCS v 3.1 and dsp6713

i have error that expected a declaration?????

this is my code:
        .bss    output,40   error here
        .bss     buffer,40
   
coeff    .short    0x7e66

y1        .short    0x1209
       
        MVKL    .S1        coeff,A0
        MVKH     .S1     coeff,A0
        LDH     .D1     *A0,A2       
        MVK     .S1     0x0001,A0     //setup circular buf AMR=0001_0001h
        MVKLH     .S1     0x0001,A0     //; setup circular buf AMR=0001_0001h
        MVC     .S2     A0,AMR      
        MVKL    .S1     output,A3  
        MVKH    .S1     output,A3
        MVK     .S1     0,A0
        STH     .D1     A0,*A3++    
        MVK     .S1     buffer,A4
        MVKH    .S1     buffer,A4
        MVK     .S1     y1,A0
        MVKH     .S1     y1,A0
        LDH     .D1     *A0++,A1     //; load y1
        NOP             4
        STH     .D1     A1,*A4++    
        STH     .D1     A1,*A3++    
        LDH     .D1     *A0,A1        
        NOP             4
        STH     .D1     A1,*A4++    
main:     MVK     .S1     40,A1        
loop:     LDH     .D1     *A4++,B1    
        LDH     .D1     *A4,B2        
        NOP             3             //; <–– try optimizing here
        MPYSP     .M1     A2,B1,A0   
        SUB     .L1     A1,1,A1
[A1]     B         .S1     loop
        SSUB     .L2X     A0,B2,B0   
        STH     .D1     B0,*A4        
        STH     .D1     B0,*A3++   
        NOP             5