This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DRV8301-HC-C2-KIT: Code COmposer Studio

Part Number: DRV8301-HC-C2-KIT


Tool/software: Code Composer Studio

I'm new to CCS. Im working on sci_echoback program. I used hyper terminal to read the data and it is working properly. This I can achieve only when I connect the controller kit to Code Composer Studio IDE and I've to run (debug mode) the code. Is there a way to make the dsp standalone? That is, my program should run immediately after power on(without connecting dsp to ccs).(cold start and hot start)

Thank you