This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Running multiple eZdsps F28335

Hello,

Can anyone, please, point out a document that describes the steps required to install and run two eZdsp F28335 on the same computer, simultaneously?

So far I installed the boards; everything is fine when only one is powered, but when I power up the second one Windows Device Manager gives an error: Windows cannot load the device for this hardware because there is a duplicate device already running in the system (Code 42). For installation I used the CD that comes in the box.

Where can I find the relevant information on running multiple eZdsps?

Thank you,

Cristian.

 

  • Cristian,

    Did you check with Spectrum Digital if this is possible? Although I couldn't find anything that says the contrary on their support pages, I am not sure if identical eZdsp kits are supposed to run simultaneously on the same host PC.

    You may try to use the procedure listed on their document that talks about how to connect multiple XDS510USB emulators:

    http://support.spectrumdigital.com/guides/files/SdTechNote_4_24001.pdf

    Hope this helps,

    Rafael