This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC3235S: LAUNCHXL-CC3235S

Part Number: LAUNCHXL-CC3235S
Other Parts Discussed in Thread: CC3235S

Tool/software: Code Composer Studio

This Launchpad LAUNCHXL-CC3235S does not appear in Kits and Boards subdirectory of Development tools directory of TI Resource Explorer, although it is detected when connected. Furthermore project examples do not appear and do not have access to any related project. When I installed CCS version 9.3.0.00012 I chose TI MCU's including Hercules and Sitara, but not 2000. Therfore I have not been able to start using CCS for this LaunchPad. Best Regards , César Castellanos, mail divertech07@gmail.com 

  • Cesar,

    For CC3235S the examples are part of the SimpleLink CC32xx SDK which is under Software:

    To be able to import and use these examples you need to have installed support for SimpleLink CC32xx

    If you did not select to install SimpleLink Wi-Fi CC32xx you can just run the installer again and point it to your existing installation.

    Regards,

    John