Other Parts Discussed in Thread: CCSTUDIO
Hi all,
I am working with LYRTECH PADK C6727 350MHz When I tried to connect the hardware using USB I am getting an error while installing the driver, I follow the procedure from get start guide.
When I select that ltpadk_usb.inf file it shows The specified location does not contain ant information about your Hardware.
So I tried with XDS510USB emulator in that when I test the emulator I am getting this message
** Using emulation application from directory c:\ccstudio_v3.3\drivers
**Emulator is reset
** Using emulation application from directory c:\ccstudio_v3.3\drivers
** Checking for a valid emulator/eZdsp
$$ You are connected to:
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Checking emulator/eZdsp scan connection
** Emulator Test **
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Emulator Scan Test
-- Found JTAG IR length of 10
-- Found 1 JTAG device(s) in the scan chain
Here I am getting the JTAG IR length of 10 and only 1 JTAG device found in the scan chain. But it should be length of 54 and 2 JTAG device.
After this I try with CCS3.3 and XDS510USB emulator it shows the following error...
error Connecting to the target:
Error 0X80000200/-163
Fatal error during: OCS,
BAD Target silicon revision number
The number of devices in JTAG scan path
must be correct for the silicon revision to be read.
Or, you may have selected the wroing DSP device driver