I desingned a programmer as well as the baseline hardware but i can´t connect. Where are the Error, what means the Errormassage ?
Error connecting to the target: Error 0x80000240/-2082 Fatal Error during: Initialization, OCS, Device driver: Emulation Connection Loss Detected on Target CPU. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.
I/O Port = 0
Board Name: F28035 XDS100USB
Cpu Name: TMS320C2800_0
Abort: Close Code Composer Studio. Retry: Try to connect to the target again. Cancel: Remain disconnected from the target Diagnostic: Run diagnostic utility.
thx