This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: Mac Error Code in Apple

Tool/software: TI C/C++ Compiler

When a bug check is issued, a crash dump file will be created if the system is configured to create them. In case of a Mac Error Code 43, this doesn't happen. It does not let the user install or download anything, for that the important applications are bound to corrupt as backup cannot be taken, I need a solution for this issue, please provide with one.