I recently upgraded to code composer studio 4.2.1.00004. Since the upgrade I am unable to set breakpoints in the C source code windows. The breakpoints still work in the disassembly (main) window and I can flash the TMS320F28335 microcontroller with updated code, so i belive my hardware and the XDS510 USB JTAG to be working. When I try to set a breakpoint in a C source window and enable it, I get the following breakpoint manager error msg:
"No code is associated with "C:/a_long_path_chain/my_file.c" line 81 in any loaded symbols.
any suggestions on how to correct this?
Sincerely,
Jared